Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
PowerStor Supercapacitors Slide 7

Cell balancing should be used in a design to maximum system lifetime when cells are connected in series. If standby or leakage current is not critical, as in a back-up power system connected to electrical mains, a passive approach is simple and most reliable. In a system where leakage current is critical, an active approach is typically used. Passive balancing utilizes fixed resistors in parallel with each cell. In a system with cells in series and in parallel, a common resistor can be used for the cells in parallel. Active balancing monitors the cell voltage and turns circuits on to drain energy from a higher voltage cell and reduce the voltage.

PTM Veröffentlicht am:
PTM Updated on: 2021-09-30