Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
PowerStor Supercapacitors Slide 15

So now the designer will look at the next value up in capacitance which is 35 F and an ESR of 0.024 Ohms. Taking into account the environmental parameters one will have a capacitance of 24.5 F and an ESR of 0.48 Ohms. Then verify the new parameters to the initial requirements of 2.56 F and 1.75 ohms ESR buy using equations 4 and 5. Then calculate dVTotal with the new values, dVTotal is 6.0 V and this is less than the 7 V originally calculated deeming this as a valid solution.

PTM Veröffentlicht am:
PTM Updated on: 2021-09-30