Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Slide16

Wave soldering is the preferred method for thru-hole components if there is substantial volume. Typical solder temperature is 500°F or 260°C with a solder dwell time of 3 to 5 seconds. Typical preheat temperature is 266°F or 130°C, and a post process wash is required. This requires the use of a process sealed switch, to minimize the possibility of contact contamination due to the wash.

PTM Veröffentlicht am: