Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Reed Switch Basics Slide 3

Generally, a switch is a device that turns electrical current on or off. In a reed switch, reed-like blades of nickel and iron form the switching mechanism. This composition of nickel and iron is easily influenced by electromagnetic energy. A small area near the end of each blade is plated with a very conductive metal like rhodium, ruthenium, gold or a combination to provide a highly conductive surface allowing for low and stable contact resistance.

PTM Veröffentlicht am: