Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Reed Switch Basics Slide 13

Breakdown Voltage is the voltage at which arc-over will occur to an open switch. Switching Voltage is the maximum voltage that can be repeatedly applied to a switch at a specific test current and duty cycle. Duty Cycle is the ratio of ON versus OFF time. With a magnet of known strength, magnet actuation is the distance from the switch for operate and release.

PTM Veröffentlicht am: