Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
xplained
The sensors on the top boards presented on this slide differ from the sensors on the boards shown on the previous slide. The pressure sensor board holds an atmospheric pressure sensor typically used for altitude sensing with a resolution of 25 cm. The light and proximity board can be used to measure ambient light and proximity. Such features could be used to implement a motion detection application. It is likely that in the future top boards compatible with the Xplained development board will be provided not only by Microchip, but also major sensor manufacturers.
PTM Veröffentlicht am: