Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Xplained-Slide2

Sensors typically measure a specific physical effect, and provide the result of this measurement over an interface to a controller. The most common types include a gyroscope which detects rotation, normally defined as rotation around an axis (X, Y, Z); an accelerometer to detect linear acceleration, also normally defined along the axis (X, Y, Z); a magnetometer that detects strength and direction of a magnetic field, a common application is detecting earth's magnetic field when used as a compass; light sensors that detect differences in light intensities, e.g. to adjust the brightness of a display or detect an approaching object; and pressure sensors used to detect differences in air pressure in an enclosed space or altitude in the atmosphere. The common choice of input/ output interface for the low cost range of sensors is I²C. Some sensors come pre-calibrated from the factory, others need an initial calibration before being put to use. 

PTM Veröffentlicht am: