Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
SAM3U-PowerMgmt-Slide19

The SAM3U also features a clock failure detector, which allows detection of an eventual defect of the crystal, disconnection of the crystal for example. In this case, the processor will switch automatically to the internal RC oscillator and will send an interrupt to the system. The customer needs to manage the interrupt, but the response will prevent system hanging. It can also be programmed as a fault input for the PWM controller.

PTM Veröffentlicht am: