Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
SAM3U-PowerMgmt-Slide16
The SAM3U contains a new reset pin, called NRSTB, which is an asynchronous reset and acts as the power on reset cell on the chip. It resets everything on the chip and has an integrated anti-glitch filter. This is different from the NRST which can be found on all of Microchip's other devices and which resets only the core and the peripherals, but not the backup region.
PTM Veröffentlicht am: