Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
F1680 Series Slide 10

The clock block of the F1680 Series has a main system clock using an Internal Precision Oscillator (IPO). This IPO is a trimmable clock source which requires no external components, is frequency selectable from one of eight frequencies (43 kHz to 11.0592 MHz), and is available with factory-trimmed calibration data. There is also a secondary low power 32 kHz Oscillator which is optimized for use with a 32 kHz watch crystal that can be used as timer/counter clock source in any mode.

PTM Veröffentlicht am: