Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
Phototriac Slide 6

Vishay’s portfolio of phototriacs for the home offer a wide variety of zero crossing and non-zero crossing phototriacs with an equally broad selection of trigger currents, blocking voltages and packages. The parts shown in the table are just a few of the phototriacs Vishay manufacturers for consumer applications: the VO3062 (v-o-thirty-sixty two) and -3 (three), the IL410 (I-L-four-ten), the VO2052 (v-o-twenty-fifty two) and -3(three), the IL420(four twenty), and the K30 (k-thirty) series. As mentioned earlier, a phototriac is commonly used to drive a TRIAC. The power phototriac included in the table, the VO2223 (v-o-twentytwo-twentythree), integrates a phototriac and a TRIAC in a single component.

PTM Veröffentlicht am: