Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
KVM Switches Slide 10

There are two sides to every KVM switch application. The Console side includes the keyboard/monitor/mouse console used to control the KVM switch and connected servers. The installation shown on this slide is typical: one user with one console controls one KVM switch. However, the Console side can get more complex, depending on the KVM switch model and the preference of the user. Select models allow up to five users with five separate consoles to control a single KVM switch. The Server side includes the servers that the user controls through the KVM switch. Select KVM switches allow users to connect multiple KVMs together to increase the amount of servers controlled.

PTM Veröffentlicht am: