Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
TCR5AM LDO Slide 2

Toshiba’s LDO line-up with a variety of packages and output currents is shown on this slide. In addition to the functions shown they have other features, such as low quiescent current, or low PSRR (power supply ripple rejection). There are also built-in features like over-current protection, thermal shutdown, automatic output discharge, and inrush current protection. The remainder of this presentation will discuss the TCR5AM series LDO which is a dual supply, ultra-low dropout 500 mA LDO.

PTM Veröffentlicht am: