Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
What is Bluetooth Slide 7

Transmitter output power is regulated and requires certification. A Class 2 certified device will have a signal that can travel about 10 m, or about a room’s range. A Class 1 device can travel upwards of 100 m, or in an actual application, about a house’s range. There is a third power class, although not a standard, called Class 1.5. This naming was designed to denote a device that achieves increased output power without the use of an external power amplifier.

PTM Veröffentlicht am: