Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
TM4C129x ESD Guidelines Slide 5

Lastly, the ESD can also propagate to the active components though holes in a poorly designed chassis or enclosure. In such cases, it is a good idea to provide adequate grounding such that the static charges are routed away from critical semiconductor components. As a general guideline, if possible use shielded cables for connections between two enclosures. Some suggestions of routing static charges away from the active circuitry are illustrated on the diagrams shown here.

PTM Veröffentlicht am: