Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Semiconductors for Ultrasound Slide 15

The image on this slide is a blowup of the picture in the previous slide. The Spectral Doppler is the lower image and the B-mode is the image above and the color is the color flow overlay on top of the B-mode image. Looking at the Doppler image at the bottom, the scrolling spectral display indicates flow velocity on the X axis while the Y axis is time. The intensity of the image shows the strength of the flow of blood.

PTM Veröffentlicht am: