Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
LM20K Family PowerWise Synchronous Buck Regulator Slide 25

The waveform to the right shows two cases; both cases assume the output voltages and currents are the same for simplification. The first case shows the switch currents and input capacitor current when two converters are connected to a common bus with no phase shift in the operating frequencies. As can be seen, the input capacitor will have to handle a huge ripple current. To hold the input more stable, the value of the input capacitor would need to be doubled. The second case shows the same converters running with a phase shift of 180 degrees in the oscillator frequency. This phase shift can reduce the ripple current allowing the use of fewer or smaller input capacitors.

PTM Veröffentlicht am: