Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
MSP430FR5969 LaunchPad Part 6 Slide 3

The goal of this lab is to sample an analog input channel A2. The start of conversion is controlled in software. The conversion result is analyzed to see if the input voltage is above or below 1/2Avcc. An LED is turned on or off based on the result. In the next lab, the engineer will modify the settings used here but make the code more efficient for ultra-low power operation. This slide lists the different settings that need to be configured in this lab.

PTM Veröffentlicht am: