Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
LaunchPad Temboo Integration Slide 6

An important advantage of Temboo’s IoT Mode in programming connected devices is its simple dropdown interface for customizing generated code to work with specific hardware and local networks. The code generated in IoT Mode will be ready to run on the device and network specified without any additional manipulation by the programmer. Moreover, a device configuration specified in IoT Mode can be saved and reused when generating code for any of the Choreos in the Temboo Library. All Temboo Choreos and the inputs that they take are also thoroughly documented on the Temboo website with explanations of tasks, sample outputs, and external links.

PTM Veröffentlicht am: