Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
USB-to-Serial Bridge Implementation Using the TUSB3410 Slide 6

The same drivers are used for both Windows Vista and Windows XP. In addition to using the header generator tool to modify the EEPROM image file, changes also need to be made to the .INF file. This text file is used by the OS to determine what it “knows” about a hardware device at plug-in (or enumeration). The information in the INF file must match that in the header of the EEPROM image.

PTM Veröffentlicht am: