Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
FB Series Slide 5
This slide shows the electrical specifications including the electrical schematic and the performance data of the Corcom FB Power Line Filters. Electrical Specification include the maximum leakage current, the highpot rating values for one minute, rated maximum voltage, operating frequency and the rated current. Minimum insertion loss values for common and differential mode measured in a closed 50 Ohm system over the frequency range from 30 kHz to 30 MHz. All these details can be obtained from the data sheet on the Corcom website at corcom.com or the TE Connectivity website at te.com.
PTM Veröffentlicht am: