Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
DRF-Slide10

To fit the DRF unit to the DIN rail, tilt the unit and push downward until the unit hits the stop. Push the bottom front side to lock it on the rail. Rock the unit lightly to verify that the lock is secure. To remove the DRF unit, either push down on the upper tab or rotate a flat blade screwdriver in the lower tab. Gently lift the lower front edge and remove the unit.

PTM Veröffentlicht am: