Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Small Motor Drivers Slide 3

The electronically commutated motors all have a very similar block diagram of the control and drivers. For any of the motors there is some power conditioning circuit that supplies a DC voltage for the drive stage, this may be as simple as a rectifier and capacitor for some of the larger motors or may be a switching power supply to generate a lower voltage for some of the smaller motors. Generally the control is implemented in a microcontroller and that interfaces to the power stage. In the block diagram shown here, gate drive IC’s provide the interface between the power MOS or IGBTs and the control logic.

PTM Veröffentlicht am: