Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Gate Drivers Overview Slide 12

The smart shutdown feature works in conjunction with the fault comparator. Previously, gate drivers have only a shut down pin with an RC circuit connected to provide a delay during power up. In the event of an emergency condition (over current for instance), this RC circuit also delays the shut down of the application. Therefore a trade-off must be found between the time to power up an application and the time to shut down. The smart shutdown function avoids this trade off. The comparator detects a fault condition and switches an internal MOS to shut down the gate drivers independently of the RC circuit. Hence, a long power up and a short shut down is possible.

PTM Veröffentlicht am: