Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
Digital MEMS Microphones Slide 14

Most bottom-port microphones have very similar designs. As the name implies, the sound inlet is on the bottom, and the sensor is placed directly over the sound inlet. This creates a small front chamber that provides good high frequency response, and a large back chamber, which gives good low frequency response and good sensitivity. The difference between ST and the competitors when evaluating bottom-port microphones is primarily a function of the differences in the sensors that are being used.

PTM Veröffentlicht am: