Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Product List
CINT1200 AC/DC Power Supplies Slide 4
The low profile CINT1200 can easily fit in 1U height products. With 200 Watts capability, from 90 to 264 VAC, it can provide total power required by most devices to run the respective system. Thus eliminate the need for secondary supply to run motors or fans. Delivering almost all of its maximum power (180 W) and not having to use a fan to operate the power supply is a major benefit to end-applications. In terms of reliability, fans are the major single point of failure in electronic assemblies. Throughout the life of the product, the fan could get replaced two to three times. Besides the cost of the fan itself, sending out a technician or recalling the product is very costly. The noise generated by fans is also not an attractive feature and in places that more than one device is on at one time, it can be a serious environmental issue. Using the CINT1200 power supply to run a device can eliminate the issues with fans and provide a marketing edge for end applications.
PTM Veröffentlicht am: