Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
CP21xx USB Bridge Slide 8

The latest additions to Silicon Labs’ industry-leading Smart Interface family are the CP2104, CP2105, CP2110 and CP2112 connectivity bridges. These devices extend their portfolio to include cost-sensitive USB to UART, USB to Dual UART, HID-USB to UART and HID-USB to SMBus\I²C bridge solutions. Common to all these devices are royalty-free software driver suites, crystal-less operation, in-system programming memory and small 4 mm x 4 mm packages that in combination reduce cost, simplify design and shorten development time. In addition, Silicon Labs is uniquely positioned to be the only supplier able to offer HID-USB to UART and SMBus\I²C solutions (CP2110 and CP2112). Also, HID-USB class solutions have been added to the smart interface family, eliminating the need for drivers, offering seamless compatibility with most operating systems and delivering significant savings and time to market advantages.

PTM Veröffentlicht am: