Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Wi-SUN Operating Specifications

The Wi-SUN operating specification shown in the table here has a list of standards organized in rows and communication protocols organized in columns. Wi-SUN has significant advantages over other communication protocols, such as: no direct services are needed, worldwide standards, fast data rates, and hopping capabilities. Now, take a look at the other graph on the bottom left of the slide. The horizontal axis is the communication distance, and the vertical axis is the communication speed. Wi-SUN operates at around 100 kB/s at 1 km, which is right in the middle of Wi-Fi and LoRa. It is the most widely used radio in IoT because of its well-balanced specifications. Like Wi-Fi, Wi-SUN is organized by a standardization which allows products to be interoperable. This interoperability ensures Wi-SUN to work great for large-scale networks, and the hopping capability even allows connections in places that have many obstacles.

PTM Veröffentlicht am: