Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Slide 58 Slide 59 Slide 60 Slide 61 Slide 62 Slide 63 Slide 64 Slide 65 Slide 66 Slide 67 Slide 68 Slide 69 Slide 70 Product List
Electromagnetic Noise Reduction Slide 49

We have already discussed the fact that the main system clock can be an important source of noise as it drives the ICs in a system. The same comment holds true inside the microcontroller. One important EMI-reduction approach MCU designers can take to reduce EMI is to change the driving capability of the clock oscillation circuit to match the changing needs of the on-chip peripherals, accommodating varying operating conditions, including differences in Vcc levels and CPU frequencies. As was the case on a system level, the goal is to prevent clock signal overshoot and undershoot, and smooth the transitions. A dual-drive-mode clock oscillator circuit is used in Renesas M16C MCUs. It starts up with a larger, more powerful buffer amplifier (A) to get the oscillator started reliably, and then switches to a smaller buffer amplifier (B) when appropriate to sustain the steady-state oscillation and generate minimum EMI.

PTM Veröffentlicht am: