Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List Associated Content
Image of Renesas CK-RA6M5/CK-RX65N Cat-M1 Cloud Kits with RYZ014A PMOD -  Cloud Certification Link1

Certification ensures reliability of the software and hardware of the kits all the way up to the software applications. The FreeRTOS example shows the software configuration of AWS FreeRTOS and the scope of support from Renesas FSP/FIT platforms. Certified software implies that the whole application is certified through all the layers of the stack and the user can modify the application layer with confidence that the lower layers are stable.

PTM Veröffentlicht am: