Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Product List
Features Continued - 1

The reason why the P4SP is able to carry such high current is due to its very low contact resistance across the pins. Although the maximum rating is 40 mΩ, the typical value below 20 mΩ which is less than half of the previous generation. Also, due to stable contact resistance of this connector, an analog signal transmission is also possible without unwanted waveform deformations.

PTM Veröffentlicht am: