Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Serial GPIO Peripheral Slide 11

NXP’s “lpcware.com” site is an engineer to engineer community, hosting these downloadable resources as well as active discussion forums. Application notes and code examples are available for the Serial GPIO use cases described in this training. Implementations of PWM waveform generation, UART emulation, SPI emulation, and an 8-bit color camera interface are provided. These examples include both the source code and documentation to provide engineers with everything they need to demonstrate SGPIO capabilities. Visit the LPCware.com site to learn more about applications of the SGPIO peripheral, and designing with NXP’s LPC line of microcontrollers.

PTM Veröffentlicht am: