Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
Arc Detect

The SA614AHR is used for Arc Detect Circuit Breaker applications. The SA614AHR is an IF subsystem in the HXQFN16, a 3 mm by 3 mm package. It is used to detect the noise spectral signal on the AC power lines caused by an arc fault condition. The RSSI output signal is analyzed by the microcontroller which executes the system safety protocols that result in tripping the AC circuit breaker.

PTM Veröffentlicht am: