Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
coldfire-embedded-slide6

This graphic illustrates what an overall VoIP solution looks like. On the left is the actual voice, which is either produced by the speaker or picked up by the microphone. This feeds into the analog codec, which is basically the analog-to-digital and digital-to-analog conversion that is done in an external audio codec. The information is then passed over the SSI interface to the processor, where the voice has to be either compressed or decompressed to limit the amount of network bandwidth that is necessary to transmit the voice information.

PTM Veröffentlicht am: