Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
RF-Slide6

Moving air creates audible noise and as fan performance and speed increases so will noise. The high performance aerodynamic designs used in NMB’s R and F Series allow them to run at lower speeds than would typically be needed to give such high flow rates, which in turn means lower noise. The design also focuses on reducing airflow turbulence and minimizing audible tonal peaks; two techniques which help make fan noise signature less intrusive to the human ear.

PTM Veröffentlicht am: