Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
M2M-Slide9

General Packet Radio Service or GPRS is a service on the 2G and 3G cellular communication systems (GSM). GPRS provides data rates of 56-114 kbps, which provides users with the capability to connect to the Internet. This can be used for systems needing email, or simple internet communication. Common protocols included in the LEON-G200 are SMTP, HTTP, and FTP. Simple Mail Transfer Protocol (SMTP) is an e-mail transmission across Internet Protocol or IP networks. HTTP or Hypertext Transfer Protocol is a networking protocol for distributed, collaborative, hypermedia information systems. HTTP is the foundation of data communication for the World Wide Web. The M2M board can pull data off the Internet and store it in its 1Mb of memory automatically. All the program has to do is read the data from memory when the program needs it. FTP or File Transfer Protocol is a standard network protocol used to copy a file from one host to another over a TCP-based network, such as the Internet.

PTM Veröffentlicht am: