Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
EEPROM-Slide8

To prevent this, a pull-up resistor is connected to the controller with the WP pin as shown on this illustration. This setup prevents writes during power-ups and power-downs by always keeping the WP pin high when the pin is not explicitly driven. When a write is actually required, the WP pin must be driven to logic 0 by the master which adds a degree of protection to the design by using just one resistor and one MCU pin.

PTM Veröffentlicht am: