Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
LDO FAQs Slide 10

What is the accuracy of my LDO? The accuracy of the LDO is the VREF (ADJ) voltage accuracy. It is typically 1% at certain conditions. If a resistor divider is used for an ADJ device, the total accuracy will be affected by the external resistance tolerance. For example, if the resistors have 1% tolerance each (worst-case), the accuracy of the output is about 3% (2% for external resistors, 1% for VREF accuracy). For the single-resistor LT308x LDO family, the total accuracy is 2% (1%+1%) for all output voltages.

PTM Veröffentlicht am: