Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
LTC4282-Slide5

For low stress staged start, a small economical MOSFET, Q1, is selected for the stress path, lowering total MOSFET cost. The inrush current level is set to a few amps with a resistor-capacitor combination on Q1’s gate. Q1 is protected with a low current limit by selecting a large sense resistor. Load current and MOSFET Q2 are held off at startup with GPIO1 configured as a power good signal. Q1 trickle charges the load capacitance over a long period of time spanning tens of milliseconds, lowering the startup stress. After the output charges and power good goes high, the parallel RDS(ON) path with Q2 is enabled to carry the full load current. During current limit or input voltage steps, the RDS(ON) path may not turn off if the output voltage does not fall below the power good threshold. Hence, a short fault timer is chosen to protect Q2. Therefore, the low stress configuration has limited ride-through capability for load surges and input voltage steps, and cannot start into a load.

PTM Veröffentlicht am: