Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
ART-Slide4

The ART is a pure Rogowski coil, and there are no additional trimming resistors or other components which provides stability over the product’s lifespan. LEM has designed its own winding machine which allows for compensation in any fluctuations in the diameter of the inner insulator which improves the accuracy of the output. The ART also includes an internal electrostatic shield to help eliminate noise from the output.

PTM Veröffentlicht am: