Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
Configurability

The 2CCP configurable platform allows users to select the best option for their application but keeping the same housing footprint. The 2CCP offers dual direction cable spans, but the customer has the option to order a single span with either a left side or right side cable. Optional features include an improved LED with more light intensity and better side viewing to ensure long distance visibility. The optional E-stop button provides access at the extreme ends of the span. The integrated restart button option can be used to provide a signal back to the PLC for equipment start. This saves the need to install a local control station or using an existing HMI.

PTM Veröffentlicht am: