Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
zx-slide13

ZX plugs come in two different types, direct solder and solder-to-PCB. Please note: there are several components that make up an assembly. There is the ZX40-B-5S-UNIT(01) insert/interface, a ZX40-B-SLDA top shield and ZX40-SLDB bottom shield. Each one of these components are needed to make a complete assembly. On the PCB type, the wires in the cable are soldered to the PCB and then the PCB is soldered to the ZX40-B-5S-UNIT(01) insert. Using the PCB type reduces assembly time. 

PTM Veröffentlicht am: