Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
POL-Slide15
OmniOn Power is the inventor of the Tunable Loop™ feature that offers great performance at lower cost. The Tunable Loop feature allows the user to add small external components to the existing pins of a module in order to adjust the compensation characteristic. This means that the same module can be used in applications with high transient requirements. This also allows the user to optimize the application using the lowest number of external capacitors; a feature which allows for cost and space reductions while enhancing reliability.
PTM Veröffentlicht am: