Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
founded
The multi-solution approach refers to NXP’s software offering structure, as supported by the BeeKit software development tool. BeeStack is NXP’s ZigBee compliant software stack offering. The multi-solution approach is based on the Open System Interconnection (OSI) model, a networking framework for implementing protocols. In the OSI model, control is passed from one layer to the next, starting at the hardware layer and working up to the application layer and back. NXP’s multi-solution offerings work similarly. This foundation provides a common framework across NXP’s software solutions: the Simple Media Access Control (SMAC) layer, the 802.15.4 Media Access Control (MAC) solution, and the fully-compliant ZigBee solution. The structure offers designers the ability to reuse knowledge developed by using BeeKit from solution to solution, thereby reducing the need to learn multiple software tools from the bottom up. The BeeKit works in partnership with microcontroller compiler solutions to set up the radio and develop application software respectively.
PTM Veröffentlicht am: