Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Slide30

In summary, in the event of an electric or hybrid vehicle service or maintenance call the capacitors within the DC power module must be fully discharged. This is one of the areas where the PTC-ICL thermistor plays a critical role, in the draining of the charging system. The PTC-ICL for the application of the charging and discharging of the battery packs in a hybrid electric or electric vehicle are designed to replace a fixed power resistor in the circuit in order to absorb the currents during a failure mode situation. Two common main failure modes involving a DC-Link circuit are an open circuit condition in the capacitor and a failure in a relay or a switch. The PTC-ICL device is designed to absorb this energy and cut off the circuit.

PTM Veröffentlicht am: