Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
sealed anti

E-Switch offers one of largest selections of anti-vandal switches in the marketplace. The PV line is rated IP65 with the exception of the PVL pilot lamp indicator, which is rated IP67 along with the ULV line. The ULV line is UL certified as well. The PV and ULV lines provide long life and both offer illumination options with the exception of the PV2, PV3, and PV5. Popular use for the sealed anti-vandal switches include various types of vending kiosks, ticket dispensers, security devices, industrial controls, medical equipment and audio/visual equipment.

PTM Veröffentlicht am: