Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Enabling Remote Devices Overview Slide 10

The WiFi MiniCore offers both WiFi and Ethernet, which function concurrently. This opens up the possibility to create a lost cost access point with further software development. There are a number of additional features on the Rabbit 6000-based WiFi module compared to the previous RCM5600W version. These features include a greater throughput performance which on average is about 5X faster. The new modules will also support the highest levels of WiFi encryption including WPA2 Enterprise.

PTM Veröffentlicht am: