Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
just how
Since the environment can cause an infinite number of water hazards, the industry rates Degree of Protection on a scale, and CONEC Sealed D-subs are rated as IP67. That is a very tough environment for electronic devices, and only continuous submersion could be worse, and fortunately, unlikely for the target market. The industry agreed-upon test is immersion in water for 30 minutes, at a depth of 1 meter, with no air/water leakage.
PTM Veröffentlicht am: