Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
Sealed-Switch2-Slide3

Degrees of protection against solid foreign objects indicated by the first characteristic numeral. The protection against the ingress of solid foreign objects implies that the object probes up to numeral 2 shall not fully penetrate the enclosure. This means that the full diameter of the sphere shall not pass through an opening in the enclosure. Object probes for numerals 3 and 4 shall not penetrate the enclosure at all. Dust-protected enclosures to numeral 5 allow a limited quantity of dust to penetrate under certain conditions. Dust-tight enclosures to numeral 6 do not allow any dust to penetrate.

PTM Veröffentlicht am: