Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
image reject mixer

The image reject signal chain consists of two mixers, with their RF input ports driven from a splitter. Half of the source power will be delivered to each mixer RF input port (1 and 2). The LO ports are fed by a quadrature LO source. The in phase LO source drives the in phase mixer, sometimes called the I mixer. The quadrature (Q) mixer LO source is shifted 90 degrees from the I mixer LO source. The IF ports of both mixers (3 and 4) drive a 90 degree hybrid, which phase-shifts the Q IF signal and then combines the I and Q signals at the IF output (5).

PTM Veröffentlicht am: